Solid Edge 2024 Update 8 Announcement

2024-09-03T15:27:58Z

Summary


Details

September 03, 2024

Dear Solid Edge Customer:

Solid Edge 2024 Update 8 is now available for download.

We appreciate your continued business and participation in the software support process. Your feedback helps us improve Solid Edge and better serve your business needs.

Sincerely,

The Solid Edge Team

============

Release Notes:

============

Solid Edge 2024 Update 8

Version: 224.00.08.04

Download Solid Edge 2024 (2310) Updates

If clicking the direct download URL does not resolve in your browser, please go ahead, and navigate from the top-level Support Center.

===============

Email Notification:

===============

To receive direct email notifications for Solid Edge Updates, navigate to your Support Center Profile (https://account.sw.siemens.com/profile, scroll to Newsletter Subscriptions, and check the box for Software Field Bulletin

==========================================

This Solid Edge Update resolves the following PRs:

==========================================

===Assembly===

PR 11057854: Assembly Replace Part constantly breaks relationships.

PR 11095576: Random crashes resolved based on Crash log data.

PR 11103200: Hide assembly pattern hides the entire model.

PR 12034653: Creating an assembly feature on a Frame causes a crash.

PR 11064085: Assembly pattern placed occurrences for suppressed occurrences.

PR 11065544: Upload failure when extending standard parts.

PR 11113130: The display of a .rcs point cloud is not displayed correctly.

===Draft===

PR 11082911: Solid Edge crashes when starting Inspector.

PR 12036356: Huge delays in Draft when using the parts list command

===Part/Profile/Sheetmetal===

PR 10913148: The menu bar has become slower when creating sketches.

PR 11097788: Unable to save a file.

PR 11098806: Solid Edge crashes when opening properties of a PMI text box.

PR 11099361: The file cannot be saved after undoing a mirror copy part of the surface body.

PR 12036008: Physical properties are not updated in the variable table.

===SEEC===

PR 11080093: Wire harnesses and Weldments are not visible in the Teamcenter lifecycle viewer.

PR 12028111: The customer observed a crash while generating a preview image in the draft environment.

PR 11084942: Executing a custom Add-in tool in Solid Edge 2024 MP5 results in a fatal error.

===TechPub===

PR 12016350: "Publish HTML" does not support Korean file names.

PR 12033687: The first template in the Page template list is not working.

PR 12034610: Images are not displayed correctly after opening an additional .qsd file.

PR 12034804: Time delay in a group Animate steps sequentially in HTML.

PR 12035319: Selecting parts in an Exploded View using the Search tab does not work.

===Translators===

PR 12031774: JT Options Version settings 11.2 & 11.4 do not work.

PR 12033693: Migrated top-level assembly is missing parts.

PR 10979064: IFC Import is very slow

PR 10877765: Unable to create more than one 3D Print at a time

KB Article ID# PL8809293

Contents

SummaryDetails

Associated Components