Solid Edge Fixing Windows Explorer File Association Issues in Solid Edge ST9

2024-09-02T10:30:03Z
APPLICATION

Summary


Details

When double-clicking or selecting "Open" from the right-click menu in Windows Explorer, Solid Edge file types (.par, .psm, .asm, .dft, .pwd, .cfg) may not open with Solid Edge as expected. Instead, they may open with the wrong application or fail to open altogether due to incorrect file associations.

Solution

Download and run the following registry file to reset the Windows Explorer file associations for Solid Edge:

reset_solid_edge_extensions_ST9.reg (26.1 KB)

After running the script, reboot your workstation to ensure the changes take effect.

Notes

KB Article ID# PL8809045

Contents

SummaryDetails

Associated Components

APPLICATION: OTHER