Tecnomatix Controllers for KUKA_KRC_BMW

2024-08-30T07:14:59Z

Summary


Details

Dear Siemens Digital Industries Software Customer,

We are pleased to inform you that Tecnomatix controllers for "KUKA_KRC_BMW"
are available for download from https://support.sw.siemens.com.

See Tecnomatix__changes_log.html for details concerning this update.
Note: This file is located in the 'Robot Controllers Change Logs' folder directly under the 'Tecnomatix Robot Controllers' folder.


Use the following steps to download:
- Login to https://support.sw.siemens.com
- If you do not have an account, click 'Register Now' and fill out the information.
- Once on Support Center, if you do not see Tecnomatix under 'My Products', click 'Manage Products'.
- Scroll down and toggle On the Tecnomatix product.
- Scroll back to the top and click Support Center in the breadcrumb.
- Select 'Tecnomatix' from 'My Products'
- Select 'Download'
- Select Tecnomatix 17.0, 2206, 2301, 2307, 2402 or 2408
-Select Tecnomatix 17.0 Robot Controllers, Tecnomatix 2206 Robot Controllers, Tecnomatix 2301 Robot Controllers, Tecnomatix 2307 Robot Controllers, Tecnomatix 2402 Robot Controllers or Tecnomatix 2408 Robot Controllers
[Or Select 'Additional Downloads' / 'Older Versions' to access 16.1, 16.1.1 or 16.1.2]

Download the file(s):

Tecnomatix_16.1_KUKA_KRC_BMW_64BIT_v5.3.5_29_08_2024.exe

Tecnomatix_16.1.1_KUKA_KRC_BMW_64BIT_v5.3.5_29_08_2024.exe

Tecnomatix_16.1.2_KUKA_KRC_BMW_64BIT_v5.3.5_29_08_2024.exe

Tecnomatix_17.0_KUKA_KRC_BMW_64BIT_v5.3.5_29_08_2024.exe

Tecnomatix_2206_KUKA_KRC_BMW_64BIT_v5.3.5_29_08_2024.exe

Tecnomatix_2301_KUKA_KRC_BMW_64BIT_v5.3.5_29_08_2024.exe

Tecnomatix_2307_KUKA_KRC_BMW_64BIT_v5.3.5_29_08_2024.exe

Tecnomatix_2402_KUKA_KRC_BMW_64BIT_v5.3.5_29_08_2024.exe

Tecnomatix_2408_KUKA_KRC_BMW_64BIT_v5.3.5_29_08_2024.exe



To Install:

Place Tecnomatix___NNBIT_vVV_MM_DD_YYYY.exe into a folder ($Tecnomatix/downloads is suggested, where $Tecnomatix is the full path to the Tecnomatix installation).

Run Tecnomatix___NNBIT_vVV_MM_DD_YYYY.exe.

The default installation point is C:\Program Files\Tecnomatix.


If you have any issues with the installation or support of these fixes,
please contact your local GTAC support group.

Sincerely,

Siemens Digital Industries Software

KB Article ID# PL8808808

Contents

SummaryDetails

Associated Components