Solid Edge SEEC: Solid Edge is not able to connect to Teamcenter.

2024-08-27T21:16:01Z
DOC_MANAGEMENT

Summary


Details

When opening SE and go to settings --> options.... we get a message. "Solid Edge is not able to determine the Connector's local folder".

Solution

The client is set up to use Solid Edge Data Management (SEDM), used for file storage management. 

To integrate with  Teamcenter you need to set your client to use Solid Edge Embedded Client (SEEC).

See page 3.4 in the SEEC administrators guide:   →Choose PDM Integration

https://docs.sw.siemens.com/en-US/doc/246738425/PL20220830878154140.SEECAdminGuide?audience=external&pk_vid=fb7daf451e326b5ce13a8dcdffd1707e1718295444a68d41

KB Article ID# PL8808379

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC