Comma "," cannot be set as the initial value for tolerance value symbol

2024-08-26T23:11:42Z

Summary


Details

In PMI settings, I set "," as Decimal Delimiter for dimension text, but it is not reflected in Tolerance Value symbol in Feature Control Frame.
Reproduced Steps:
1. File > Preferences > PMI > Dimension > Text > Units > Decimal Delimiter = “,”



2. PMI tab > Feature Control Frame


Solution

This behavior is working as designed in NX, and the setting of Decimal Delimiter does not apply to Feature Control Frame.
Workaround : modify the symbol manually every time

Notes

There have been several enhancement requests (8649742, 10668142, 11021321, etc.) filed to set Decimal Delimiter.

**Please refer to PL8807756 for Japanese article.

Release Versions
  • NX V2206
  • NX - DRAFTING V2206
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8807758

Contents

SummaryDetails

Associated Components