Curves lose view dependency after project command

2024-08-26T23:09:41Z

Summary


Details

Lines created with Extract Curve (legacy) have view-dependent information, but if running Project Curve command on them, the view-dependent information is lost if Preview is ON.

Reproduced Steps:
1. Prepare a model
2. Menu > Insert > Derived Curve > Extract Curve(Legacy)
 If you don’t find the command, please search it in Search Window
3. Select the extracted curve > Ctrl+i > Please confirm that "View Dependent In" information is written in the Information window.



4. Menu > Insert > Derived Curve > Project
- Associative = OFF
- Input Curves = Keep, Hide or Delete
- Preview = ON



5. Select the projected curve > Ctrl + i > Please confirm the Information window to make sure there is no "View Dependent In".


Solution

This behavior is due to NX problem and will be fixed in NX 2412.
Workaround:
When performing Projection command, set "Preview" Off.

Notes

The problem occurs when all three conditions described in step 4 are met.

**Please refer to PL8807754 for Japanese article.

Release Versions
  • NX V2306
  • NX - DESIGN V2306
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8807755

Contents

SummaryDetails

Associated Components