Troubleshooting Solid Edge Crashes Using Safe Mode

2024-08-21T16:13:34Z

Summary


Details

Users may experience frequent crashes or instability when using Solid Edge. The causes of these crashes can vary, including issues with third-party add-ins, custom settings, hardware acceleration, or other external variables. Identifying the exact cause of the crash can be challenging without a systematic approach.

Solution

Running Solid Edge in Safe Mode can help troubleshoot and resolve these crashes by providing a controlled environment that minimizes external variables. Safe Mode temporarily disables certain functionalities, making it easier to isolate the issue.

Steps to Start Solid Edge in Safe Mode:

1. Close all running instances of Solid Edge.

2. Press Win + R to open the Run dialog box.

3. Type cmd and press Enter to open the Command Prompt.

4. Navigate to the Solid Edge installation directory (default: C:\Program Files\Siemens\Solid Edge \Program).

5. Type edge.exe /safe and press Enter.


Functionality Disabled in Safe Mode:

1. Add-Ins: Third-party add-ins and custom extensions are disabled. This prevents interference from these components, which may cause crashes.

2. User Settings: Certain user settings and configurations are reset to their default state, helping determine if custom settings are contributing to the crashes.

3. Hardware Acceleration: Disabled to identify if graphics drivers or hardware-related issues are causing the instability.

4. Enhanced Functionality: Features like the social media channels (e.g., YouTube pane) are disabled to eliminate potential conflicts within the application.

5. Simplified Environment: Running in Safe Mode reduces external variables, making it easier to identify the root cause of the issue.

Post-Safe Mode Steps:

  • Test Stability: Use Solid Edge as usual and observe its stability. If crashes do not occur in Safe Mode, the problem may be related to add-ins, settings, or hardware acceleration.
    • Isolate the Cause: Gradually re-enable add-ins, settings, and hardware acceleration one at a time to identify the specific cause f the crashes.

      Additional Information:

      Running Solid Edge in Safe Mode is an essential troubleshooting step for resolving crash issues. It provides a systematic approach to identifying and fixing underlying problems by isolating potential causes in a controlled environment.

      KB Article ID# PL8806753

      Contents

      SummaryDetails

      Associated Components