NX Constraint Options removed from Add Component Dialog

2024-09-19T12:38:46Z
NX for Design

Summary


Details

Constraint Options have been removed from Add Component dialog

Platforms
  • na windows-1064
Release Versions
  • NX V2406.7000
Solution

The Constraint User Interface has been rewritten, so that each constraint type has its own dialog. This was done to make the interaction consistent with other commands in NX and provide predictable edit behavior. The new UI can therefore no longer fitted inside another dialog like the Add Component dialog..No updates regarding these changes were included in the NX documentation, so a documentation problem report was submitted to get the changes documented.

Notes

KB Article ID# PL8806734

Contents

SummaryDetails

Associated Components

Assemblies