Solid Edge Command line to silently uninstall Solid Edge 2022 Maintenance Pack 10

2024-08-15T11:04:37Z
SETUP

Summary


Details

What is the command line to silently uninstall Solid Edge 2022 Maintenance Pack 10?

Solution

The command line for Solid Edge 2022 Maintenance Pack 10 (build 222.00.10.003) is:

msiexec /package {6C0CACD4-043C-44DD-8CB5-F4B7E60BCC97} /uninstall {6FA83A3F-3E02-46CA-896A-FB3E025D35EE} /qn+ /norestart /log C:\temp\2220010003_uninstall.log

Notes

To the parent article

KB Article ID# PL8806531

Contents

SummaryDetails

Associated Components

SETUP: INSTALL