Command line to silently uninstall Solid Edge 2022 Maintenance Pack 11

2024-08-15T11:04:30Z

Summary


Details

What is the command line to silently uninstall Solid Edge 2022 Maintenance Pack 11?

Solution

The command line for Solid Edge 2022 Maintenance Pack 11 (build 222.00.11.002) is:

msiexec /package {6C0CACD4-043C-44DD-8CB5-F4B7E60BCC97} /uninstall {EF1AB2B0-DEE3-462F-96F4-DD13FA31A3E6} /qn+ /norestart /log C:\temp\2220011002_uninstall.log

Notes

To the parent article

KB Article ID# PL8806529

Contents

SummaryDetails

Associated Components