Solid Edge Command line to silently uninstall Solid Edge 2022 Maintenance Pack 13

2024-08-15T11:04:17Z
SETUP

Summary


Details

What is the command line to silently uninstall Solid Edge 2022 Maintenance Pack 13?

Solution

The command line for Solid Edge 2022 Maintenance Pack 13 (build 222.00.13.004) is:

msiexec /package {6C0CACD4-043C-44DD-8CB5-F4B7E60BCC97} /uninstall {F4F22CAD-7DC4-4296-A6A7-7CF55678C3D1} /qn+ /norestart /log C:\temp\2220013004_uninstall.log

Notes

To the parent article

KB Article ID# PL8806526

Contents

SummaryDetails

Associated Components

SETUP: INSTALL