Solid Edge Weldment added to Teamcenter isn't using the Document Number for the item ID.

2024-08-28T13:34:48Z
DOC_MANAGEMENT

Summary


Details

The weldment and assembly have the same document number so when the data is added to Teamcenter one of the items is assigned an item id, the other uses the document number as expected.

Platforms
  • all n/a-n/a
Release Versions
  • Solid Edge V224.0
Solution

This is working as expected. Use the data prep utilities to assign a unique document number to each model file. If models with duplicate document numbers are added, Teamcenter will automatically assign an ID to the second model to go in.

Notes

KB Article ID# PL8805691

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC