NX Is NX 2007 compatible with Azul Zulu 17.0.3?

2024-08-08T16:57:52Z
NX System Administration

Summary


Details

Is NX 2007 compatible with Azul Zulu 17.0.3?

Solution

Developer 1 (NX Installation developer)

The answer I receive is usually that we are upward compatible with Java versions. A specific version is certified, but support is available for newer versions than the certified version.

Developer 2 (Main developer)

Compatible - Yes

Have we tested 2007 with 17?  - No

But that said it should work.

Developer 3

Yes.  But Azul Zulu 17.0.3 is not officially supported against the NX 2007 Series.

KB Article ID# PL8805687

Contents

SummaryDetails

Associated Components

Installation