Create a Spiral Profile Tool Path with a User Defined Tool to Finish Undercut in Contour
SolutionReview the movie above...
Please note the steps below...displayed in the attached movie.
- Create a curve that offsets exactly 1/2 the diameter of the tool (be sure the tracking point is accounted for) Please see image below.
- Create a Spiral
- Select the "Reuse Libray" tab on the "Resource Toolbar".
- Expand Reusable Object Library (Example Only).
- Expand "Inch".
- Select Spiral.
Please see image below....
- When defining the Spiral, make sure the Spiral is inside the 'Offset Curve" as seen below.
- Parameters for Spiral
r = radius of first curve of spiral
n = turns in the spiral
For this example... r = .05 n= 3
The distance from the end point of the outer spiral to the offset curve for the toolpath must be captured.
Use Optimization to create the desired formula...
This desired value - = 0.0000
Go to Optimization... set p16 Target Value to 0.000
Select the variables Tab.
r'3 - select the expression .05 (the initial value of r=.05
Set the upper limit to 1.
Note that the end point of the spiral ends on the offset curve. Please see the image below...