'PathXpres' and 'Curve segment' missing from Ribbon Bar in Solid Edge 2025

2025-03-12T16:54:52Z

Summary


Details

The commands 'PathXpres' and 'Curve segment' are not found in the Solid Edge Ribbon bar in Solid Edge 2025. 

Are they still available?

Release Versions
  • Solid Edge V225.0
  • Solid Edge V224.0
Solution

'PathXpres' and 'Curve Segment' features are still available but not visible by default in the Ribbon bar.
Recommended action: Customize the 'Ribbon bar' to expose these legacy features.

Select 'Customize the ribbon'.


Then add the commands to the environments needed.


Consequently, the commands are visible in the selected environment.


Notes

KB Article ID# PL8805235

Contents

SummaryDetails

Associated Components