Bond constraints not working

2024-08-06T00:47:41Z

Summary


Details

When a component that is constrained by a Bond is moved after being suppressed, and then unsuppressed it again, the component does not return to its original constrained state.

Reproduced Steps:
1. Create Assembly and add Bond constraint




2. Assembly Navigator > Constraints > Bond > Mouse right click > Suppress



3. Move a component ( to any location)



4. Assembly Navigator Constraints > Bond > Mouse right click > Unsuppress


Solution

This behavior is working as designed.


Workaround:
If you want to unsuppress and then resuppress a component to return it to its original position, please use other constraint types (such as Align and Touch).

Notes

Assembly Constraints:
https://docs.sw.siemens.com/ja-JP/doc/209349590/PL20230425446868577.assemblies/func_details_assy_constraints_ov

**Please refer to PL8804949 for Japanese article.

Release Versions
  • NX V2312
  • NX - ASSEMBLIES V2312
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8804952

Contents

SummaryDetails

Associated Components