Inherit the original face color with Unite command

2024-08-06T00:40:24Z

Summary


Details

After performing the Unite command on multiple solids with different colors, they are converted to the target color, but is it possible to keep the original colors of each?

Reproduced steps:
1. Create multiple solids
2. Assign a different color to each solids( Menu > Edit > Object Display > specify any color in the color palette)



3. Unite


Result:


Solution

In Modeling Preferences you can specify the inheritance source for faces modified by Boolean operation, so they will inherit their original color.

File > Preferences > Modeling > General > Display Properties > Face Modified by Boolean = Inherit from Tool Body( or Customer Defaults > Modeling > General > General > Display Properties > Face Modified by Boolean = Inherit from Tool Body)


Performing Step 2 above after setting:


Notes

This setting also applies to the various Boolean commands (Subtract, intersect), including Unite command.

**Please refer to PL8804408 for Japanese article.

Release Versions
  • NX V2312
  • NX - DESIGN V2312
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8804409

Contents

SummaryDetails

Associated Components