Users are looking for technical assistance to understand and utilize interfaces in the "igl.h" file, excluding the IGL interface. They have requested guidance, additional documentation, code examples, or resources for implementing and using the following interfaces: IGLU, IWGL, IGLControl, IGLUControl, IGLExtension, and IViewGLObject.
SolutionUnfortunately, the requested interfaces IGLU, IWGL, IGLControl, IGLUControl, IGLExtension, and IViewGLObject (except IGL) are inactive and cannot be used externally. These interfaces were originally intended for a specific context but were never fully implemented. As a result, they are considered deprecated, unsupported and will remain undocumented.
NotesThe term "sdk" stands for Software Development Kit, which is a collection of tools, libraries, and documentation used for developing software applications.