Highlighted display by Check Regions is not canceled

2024-08-06T00:18:43Z

Summary


Details

After running Check Regions command and highlighting the faces detected as sharp corners, I exited the command, but the highlighting was not canceled.

Reproduced Steps:
1. Prepare model data



2. Menu > Analysis > Mold Part Validation > Check Regions > Calculate tab > select Product Body and specify Draw Direction > click Calculate button



3. Information tab > select Sharp Corners as Check Scope > select one detected as a sharp corner > Apply > Cancel


the highlighting is not canceled


Solution

This behavior is due to a bug that has existed since NX 2306 and has been corrected in NX 2406.
The problem occurs if pressing Cancel button to exit the dialog after pressing Apply button.
Workaround: Please don't close with Cancel button.
If you press Cancel button and exit the command, you can cancel the highlighting by updating the view (Graphics window > mouse right-click > Update View).

Notes

The problem occurs each functions in Area and Face tabs. (The problem does not occur each functions in Face tab.)

**Please refer to PL8804187 for Japanese article.

Release Versions
  • NX V2306
  • NX - MOLDED_PART_DES V2306
  • NX - DESIGN V2306
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8804188

Contents

SummaryDetails

Associated Components