Build Processor Server and NX version

2024-07-30T08:02:54Z

Summary


Details

Getting an error with Build Processor Server.

+++ Failed to load am.xml file


Checking the file that the log is referring found that the version is NX2406, that means that there is a conflict with Build Processor Server versions.

User is running NX2406 BP server in NX2312


Solution

Running NX with an older version than the NX BP Server is something we don’t support.

So If clients run NX 2312 and NX BP Server 2406 it is required that they upgrade to NX 2406 or install the NX Bp Server 2312.

Both server versions can coexist as long as the are on different port numbers.

KB Article ID# PL8803978

Contents

SummaryDetails

Associated Components