Dear Siemens Digital Industries Software Customer,
We are pleased to inform you that Tecnomatix controllers for "ABB_RAPID, DEFAULT, FANUC_RJ, FANUC_RJ_JAPAN, FANUC_RJ_VW, KUKA_KRC, KUKA_KRC_BMW, KUKA_VKRC"
are available for download from https://support.sw.siemens.com.
See Tecnomatix__changes_log.html for details concerning this update.
Note: This file is located in the 'Robot Controllers Change Logs' folder directly under the 'Tecnomatix Robot Controllers' folder.
Use the following steps to download:
- Login to https://support.sw.siemens.com
- If you do not have an account, click 'Register Now' and fill out the information.
- Once on Support Center, if you do not see Tecnomatix under 'My Products', click 'Manage Products'.
- Scroll down and toggle On the Tecnomatix product.
- Scroll back to the top and click Support Center in the breadcrumb.
- Select 'Tecnomatix' from 'My Products'
- Select 'Download'
- Select Tecnomatix 2402
-Select Tecnomatix 2402 Robot Controllers
Download the file(s):
Tecnomatix_2402_ABB_RAPID_64BIT_v5.30_28_07_2024.exe
Tecnomatix_2402_DEFAULT_64BIT_v2.142_28_07_2024.exe
Tecnomatix_2402_FANUC_RJ_64BIT_v5.4.1_28_07_2024.exe
Tecnomatix_2402_FANUC_RJ_JAPAN_64BIT_v3.3.1_28_07_2024.exe
Tecnomatix_2402_FANUC_RJ_VW_64BIT_v4.0.3_28_07_2024.exe
Tecnomatix_2402_KUKA_KRC_64BIT_v6.17.1_28_07_2024.exe
Tecnomatix_2402_KUKA_KRC_BMW_64BIT_v5.3.1_28_07_2024.exe
Tecnomatix_2402_KUKA_VKRC_64BIT_v7.13.1_28_07_2024.exe
To Install:
Place Tecnomatix___NNBIT_vVV_MM_DD_YYYY.exe into a folder ($Tecnomatix/downloads is suggested, where $Tecnomatix is the full path to the Tecnomatix installation).
Run Tecnomatix___NNBIT_vVV_MM_DD_YYYY.exe.
The default installation point is C:\Program Files\Tecnomatix.
If you have any issues with the installation or support of these fixes,
please contact your local GTAC support group.
Sincerely,
Siemens Digital Industries Software