Proximity sensor's signal doesn't work

2024-08-16T20:22:03Z

Summary


Details

The proximity sensor signal's value doesn't change when parts are in proximity.

Platforms
  • na windows-1032
Release Versions
  • Tecnomatix V2402.X
Solution

Check the setting "Activate Assigned signals only" in the Options / Simulation dialog.

When not selected, the signal should change upon proximity of the designated objects 

When selected, then the signal has to be connected to some logic such as a Logic Block or Module. 

Note this setting was added in Tecnomatix version 16.1. Before version 16.1 having the signal connected to logic was a requirement.

Notes

KB Article ID# PL8803603

Contents

SummaryDetails

Associated Components