Solid Edge Command line to silently uninstall Solid Edge 2023 Update 13

2024-08-07T13:31:27Z
SETUP

Summary


Details

What is the command line to silently uninstall Solid Edge 2023 Update 13?

Solution

The command line for Solid Edge 2023 Update 13 (build 223.00.13.005) is:

msiexec /package {79F62F18-BA5C-404C-A9BA-8C787585015D} /uninstall {DE2919E2-CF17-4640-8CCA-65FD70517311} /qn+ /norestart /log C:\temp\2230013005_uninstall.log

Notes

To the parent article

KB Article ID# PL8802804

Contents

SummaryDetails

Associated Components

SETUP: INSTALL