Solid Edge Command line to silently uninstall Solid Edge 2024 Update 7

2024-07-23T09:31:07Z
SETUP

Summary


Details

What is the command line to silently uninstall Solid Edge 2024 Update 7?

Solution

The command line for Solid Edge 2024 Update 7 (build 224.00.07.003) is:

msiexec /package {FAF68E69-27BE-4111-A3EF-245C40A1C7F2} /uninstall {62BCFE7F-BD77-4304-AAB1-6CD2A57AC6E7} /qn+ /norestart /log C:\temp\2240007003_uninstall.log

Notes

To the parent article

KB Article ID# PL8802554

Contents

SummaryDetails

Associated Components

SETUP: INSTALL