NX Switch NX versions from the Open In NX, in Active Workspace

2024-07-22T13:22:27Z
NX for Design

Summary


Details

How can you change the version of NX that starts from Active Workspace if you have multiple versions installed?

Solution

In the startNXFromAW.bat file found in …NXxxxx\ugmanager folder, add/edit the “version” switch:


Note - The version of NX that the startNXFromAW.bat is run from depends on the UGII_BASE_DIR setting.

KB Article ID# PL8802324

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX