What are the parameters to install Solid Edge Inspector silently?

2024-07-23T09:30:16Z

Summary


Details

What are parameters for a silent installation of Solid Edge Inspector and specify a custom path?

Solution

To perform a silent installation of Solid Edge Inspector and specify a custom installation path, follow the steps below: 

1.  Download the Solid Edge Inspector executable file in the required version from the Support Center Download. The File is provided as a zip file. 

2.  Extract all the contents of the zip file by right-clicking on the file and selecting "Extract All." 

3.  Navigate to the subfolder named "~\SEInspector\SEInspectorMedia" within the extracted contents. 

4.  Locate the installer file named "SolidEdgeInspector.exe" in this folder. 

5. Open the command prompt or a terminal window. 

6. Use the following command line to perform a silent installation to your desired folder: 

     solidedgeinspector /S /D=c:\Your_folder_name 

     "Your_folder_name" must be adjusted to correspond to the folder in which you want to install Solid Edge Inspector. 

Notes

- Ensure that you have the necessary permissions to install software on your system. 

- The "/S" parameter is used to indicate a silent installation, which means the installation process will not display any user interface. 

- The "/D" parameter is used to specify the installation directory or custom path where Solid Edge Inspector should be installed. 

- It is important to note that the command is case sensitive, so ensure the parameters are written in uppercase as shown above. 

- You can modify the command to meet your specific installation requirements, such as choosing a different installation path or adding other optional parameters. 

KB Article ID# PL8802046

Contents

SummaryDetails

Associated Components