What is the MAXOFF parameter used for in the holder_ascii.def file?

2024-07-18T18:07:51Z

Summary


Details

Customer is customizing the holder library functions and notes that the MAXOFF parameter is defined in the .def file, but is not being called anywhere.  What is this used for?


Solution

According to the comments in the NX2312 holder_database.dat file, that parameter is in place but not currently being used:


This field can be safely ignored until such time as a future version of NX has this parameter in use.

Notes

Text of the explanatory comments in the .dat file:

# MAXOFF - Maximum tool offset supported by this holder.
# (Not currently implemented, but defined now for future
# use.)

KB Article ID# PL8801630

Contents

SummaryDetails

Associated Components