Symptoms where Solid Edge Draft encounters low memory issues.
SolutionHistorically, various low memory issues in Draft have been isolated to printer drivers or invalid printers. To troubleshoot those problems, see if turning off ‘Include Draft Viewer data in file’ makes a difference or try changing the default printer. Unchecking the option 'Include Draft Viewer' should be temporary, as this may result in no display of draft in downstream applications, such as Tc Vis. If the data is unmanaged, please check share drives, because sometimes they become stale. Consider deleting and recreating the share drive where Solid Edge draft documents reside.
Check if this might be indeed a Solid Edge issue. This error could manifest itself when selecting objects within the drawing. For example, if the low memory message is displayed when selecting objects in a section, try recreating the section. Please provide a reproducible test case, so that development can investigate further.
NotesRef: IRs 9844599, 7756397, 10165060