Command line to silently uninstall Solid Edge 2023 Update 1

2024-07-17T08:03:55Z

Summary


Details

What is the command line to silently uninstall Solid Edge 2023 Update 1?

Solution

The command line for Solid Edge 2023 Update 1 (build 223.00.01.005) is:

msiexec /package {79F62F18-BA5C-404C-A9BA-8C787585015D} /uninstall {ECB8CE41-5D87-4A0C-AF50-9ED592AC6B61} /qn+ /norestart /log C:\temp\2230001005_uninstall.log

Notes

To the parent article

KB Article ID# PL8801281

Contents

SummaryDetails

Associated Components