Solid Edge Command line to silently uninstall Solid Edge 2023 Update 4

2024-07-17T08:03:37Z
SETUP

Summary


Details

What is the command line to silently uninstall Solid Edge 2023 Update 4?

Solution

The command line for Solid Edge 2023 Update 4 (build 223.00.04.005) is:

msiexec /package {79F62F18-BA5C-404C-A9BA-8C787585015D} /uninstall {089C69D3-53D9-477B-BC45-82F0D8B01F82} /qn+ /norestart /log C:\temp\2230004005_uninstall.log

Notes

To the parent article

KB Article ID# PL8801276

Contents

SummaryDetails

Associated Components

SETUP: INSTALL