Solid Edge Command line to silently uninstall Solid Edge 2023 Update 5

2024-07-17T08:03:30Z
SETUP

Summary


Details

What is the command line to silently uninstall Solid Edge 2023 Update 5?

Solution

The command line for Solid Edge 2023 Update 5 (build 223.00.05.006) is:

msiexec /package {79F62F18-BA5C-404C-A9BA-8C787585015D} /uninstall {4E2B467C-FE31-470A-974C-FD0A4A82C920} /qn+ /norestart /log C:\temp\2230005006_uninstall.log

Notes

To the parent article

KB Article ID# PL8801275

Contents

SummaryDetails

Associated Components

SETUP: INSTALL