Command line to silently uninstall Solid Edge 2023 Update 6

2024-07-17T08:03:23Z

Summary


Details

What is the command line to silently uninstall Solid Edge 2023 Update 6?

Solution

The command line for Solid Edge 2023 Update 6 (build 223.00.06.004) is:

msiexec /package {79F62F18-BA5C-404C-A9BA-8C787585015D} /uninstall {03428B4A-9259-4767-B29E-CEDF4E62E1A0} /qn+ /norestart /log C:\temp\2230006004_uninstall.log

Notes

To the parent article

KB Article ID# PL8801274

Contents

SummaryDetails

Associated Components