Solid Edge Command line to silently uninstall Solid Edge 2024 Update 4

2024-07-17T08:02:29Z
SETUP

Summary


Details

What is the command line to silently uninstall Solid Edge 2024 Update 4?

Solution

The command line for Solid Edge 2024 Update 4 (build 224.00.04.004) is:

msiexec /package {FAF68E69-27BE-4111-A3EF-245C40A1C7F2} /uninstall {4723504C-3683-464E-8A07-5F5ED480DEE5} /qn+ /norestart /log C:\temp\2240004004_uninstall.log

Notes

To the parent article

KB Article ID# PL8801028

Contents

SummaryDetails

Associated Components

SETUP: INSTALL