NX Different behavior when dimension a symbolic thread

2024-07-19T08:25:32Z
NX for Design

Summary


Details

Sometimes it is necessary to represent the symbolic thread without a prefix

Solution

The reason that the "M" gets presented to the Symbolic Thread callout is because the Symbolic Thread Size Prefix is set to "M" in Drafting Preferences and the provided drafting standard file.

Resetting this preference and/or customer default to blank will create callouts without the "M."

Example:




Notes

KB Article ID# PL8800175

Contents

SummaryDetails

Associated Components

Drafting