Setting the Default Member in Solid Edge Family of Assemblies

2024-07-10T11:51:21Z

Summary


Details

Users are experiencing issues when trying to set a different assembly member as the default in a Family of Assemblies (FOA) file. When selecting a member and saving the document, the selected member does not persist as the default upon reopening the file. The problem occurs under the following conditions:

  1. Selecting a member from the Family of Assemblies panel dropdown and saving the document.
    1. Selecting a member via the "Edit table" option and saving the document.
      Solution

      The observed behavior is functioning as designed in Solid Edge. Here are the steps to correctly manage the default member in a Family of Assemblies:

      1. Default Member Creation:

      • When creating a Family of Assemblies, the first member created is automatically set as the default member.

        2. Opening the FOA:

        • If the FOA is opened from Windows Explorer, it will always display the default member.
          • If the FOA is opened using the Solid Edge "Open" command, a dialog box will appear, allowing the user to choose which member to open.

            Steps to Open a Specific Member in FOA:

            1. Use the Solid Edge "Open" command instead of opening the FOA directly from Windows Explorer.
              1. In the dialog box that appears, select the desired member to open.

                This ensures that the selected member is active upon opening the document.

                KB Article ID# PL8800174

                Contents

                SummaryDetails

                Associated Components