JT 10.9 version specification explanation is not described in the document

2024-07-08T21:05:19Z

Summary


Details

Checking NX 2406 documentation, it appears that a new JT 10.9 version has been released, but its enhanced contentes are not explained in detail.

Reproduced Steps:
1. Look at the documentation for exporting JT files from NX
https://docs.sw.siemens.com/en-US/doc/209349590/PL20231101866122454.nxtojt/configuration_opts_setup_options


Solution

NX 2406 series now supports JT 10.9 version, but the details of its enhanced contents are not yet available to users.
Please note that the documentation will be updated when it is made available to users. Therefore please wait until then for further information.

Notes

JT exported with JtFileFormat = “10” will be exported in Version 10.9 as stated in the documentation, but this will not impair the ability to export in lower versions, including Version 10.6. There is no other impact, so please use the JT that outputs with JtFileFormat = “10”. Furthermore, by explicitly specifying JtFileFormat = “106” or lower version, you can output the specified version.

**Please refer to PL8799480 for Japanese article.

Release Versions
  • NX V2406
  • NX - TRANSLATOR V2406
  • NX - DESIGN V2406
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8799481

Contents

SummaryDetails

Associated Components