Dear Siemens Digital Industries Software Customer,
We are pleased to inform you that Tecnomatix controllers for "ABB_RAPID, ABB_RAPID_VOLVO, CLS_UPLOAD, COMAU_PDL, COMAU_PDL_VOLVO, DEFAULT, DUERR_ECOTALK, FANUC_RJ, FANUC_RJ_JAPAN, FANUC_RJ_VW, HHI_HRBASIC, KAWASAKI_AS, KAWASAKI_AS_SUZUKI, NC_CODE_EMBRAER, NC_CODE_RIVETING, OLP_TOOL, YASKAWA_INFORM, EFORT_XPL, ESTUN_ERL"
are available for download from https://support.sw.siemens.com.
See Tecnomatix_<ControllerName>_changes_log.html for details concerning this update.
Note: This file is located in the 'Robot Controllers Change Logs' folder directly under the 'Tecnomatix <Version> Robot Controllers' folder.
Use the following steps to download:
- Login to https://support.sw.siemens.com
- If you do not have an account, click 'Register Now' and fill out the information.
- Once on Support Center, if you do not see Tecnomatix under 'My Products', click 'Manage Products'.
- Scroll down and toggle On the Tecnomatix product.
- Scroll back to the top and click Support Center in the breadcrumb.
- Select 'Tecnomatix' from 'My Products'
- Select 'Download'
- Select Tecnomatix 16.1.1, 16.1.2, 17.0, 2206 or 2402
-Select Tecnomatix 16.1.1 Robot Controllers, Tecnomatix 16.1.2 Robot Controllers, Tecnomatix 17.0 Robot Controllers, Tecnomatix 2206 Robot Controllers or Tecnomatix 2402 Robot Controllers
Download the file(s):
Tecnomatix_16.1.1_ABB_RAPID_64BIT_v5.28.2_05_07_2024.exe
Tecnomatix_16.1.1_ABB_RAPID_VOLVO_64BIT_v5.18.2_05_07_2024.exe
Tecnomatix_16.1.1_CLS_UPLOAD_64BIT_v1.15.5_05_07_2024.exe
Tecnomatix_16.1.1_COMAU_PDL_64BIT_v5.7.1_05_07_2024.exe
Tecnomatix_16.1.1_COMAU_PDL_VOLVO_64BIT_v2.16.1_05_07_2024.exe
Tecnomatix_16.1.1_DEFAULT_64BIT_v2.140_05_07_2024.exe
Tecnomatix_16.1.1_DUERR_ECOTALK_64BIT_v2.91_05_07_2024.exe
Tecnomatix_16.1.1_FANUC_RJ_64BIT_v5.3.1_05_07_2024.exe
Tecnomatix_16.1.1_FANUC_RJ_JAPAN_64BIT_v3.2.2_05_07_2024.exe
Tecnomatix_16.1.1_FANUC_RJ_VW_64BIT_v4.0.1_05_07_2024.exe
Tecnomatix_16.1.1_HHI_HRBASIC_64BIT_v2.1_05_07_2024.exe
Tecnomatix_16.1.1_KAWASAKI_AS_64BIT_v5.34.4_05_07_2024.exe
Tecnomatix_16.1.1_KAWASAKI_AS_SUZUKI_64BIT_v1.3.4_05_07_2024.exe
Tecnomatix_16.1.1_NC_CODE_EMBRAER_64BIT_v1.17_05_07_2024.exe
Tecnomatix_16.1.1_NC_CODE_RIVETING_64BIT_v1.15_05_07_2024.exe
Tecnomatix_16.1.1_OLP_TOOL_64BIT_v16.4.3_05_07_2024.exe
Tecnomatix_16.1.1_YASKAWA_INFORM_64BIT_v6.57_05_07_2024.exe
Tecnomatix_16.1.2_ABB_RAPID_64BIT_v5.28.2_05_07_2024.exe
Tecnomatix_16.1.2_ABB_RAPID_VOLVO_64BIT_v5.18.2_05_07_2024.exe
Tecnomatix_16.1.2_CLS_UPLOAD_64BIT_v1.15.5_05_07_2024.exe
Tecnomatix_16.1.2_COMAU_PDL_64BIT_v5.7.1_05_07_2024.exe
Tecnomatix_16.1.2_COMAU_PDL_VOLVO_64BIT_v2.16.1_05_07_2024.exe
Tecnomatix_16.1.2_DEFAULT_64BIT_v2.140_05_07_2024.exe
Tecnomatix_16.1.2_DUERR_ECOTALK_64BIT_v2.91_05_07_2024.exe
Tecnomatix_16.1.2_FANUC_RJ_64BIT_v5.3.1_05_07_2024.exe
Tecnomatix_16.1.2_FANUC_RJ_JAPAN_64BIT_v3.2.2_05_07_2024.exe
Tecnomatix_16.1.2_FANUC_RJ_VW_64BIT_v4.0.1_05_07_2024.exe
Tecnomatix_16.1.2_HHI_HRBASIC_64BIT_v2.1_05_07_2024.exe
Tecnomatix_16.1.2_KAWASAKI_AS_64BIT_v5.34.4_05_07_2024.exe
Tecnomatix_16.1.2_KAWASAKI_AS_SUZUKI_64BIT_v1.3.4_05_07_2024.exe
Tecnomatix_16.1.2_NC_CODE_EMBRAER_64BIT_v1.17_05_07_2024.exe
Tecnomatix_16.1.2_NC_CODE_RIVETING_64BIT_v1.15_05_07_2024.exe
Tecnomatix_16.1.2_OLP_TOOL_64BIT_v16.4.3_05_07_2024.exe
Tecnomatix_16.1.2_YASKAWA_INFORM_64BIT_v6.57_05_07_2024.exe
Tecnomatix_17.0_ABB_RAPID_64BIT_v5.28.2_05_07_2024.exe
Tecnomatix_17.0_ABB_RAPID_VOLVO_64BIT_v5.18.2_05_07_2024.exe
Tecnomatix_17.0_CLS_UPLOAD_64BIT_v1.15.5_05_07_2024.exe
Tecnomatix_17.0_COMAU_PDL_64BIT_v5.7.1_05_07_2024.exe
Tecnomatix_17.0_COMAU_PDL_VOLVO_64BIT_v2.16.1_05_07_2024.exe
Tecnomatix_17.0_DEFAULT_64BIT_v2.140_05_07_2024.exe
Tecnomatix_17.0_DUERR_ECOTALK_64BIT_v2.91_05_07_2024.exe
Tecnomatix_17.0_FANUC_RJ_64BIT_v5.3.1_05_07_2024.exe
Tecnomatix_17.0_FANUC_RJ_JAPAN_64BIT_v3.2.2_05_07_2024.exe
Tecnomatix_17.0_FANUC_RJ_VW_64BIT_v4.0.1_05_07_2024.exe
Tecnomatix_17.0_HHI_HRBASIC_64BIT_v2.1_05_07_2024.exe
Tecnomatix_17.0_KAWASAKI_AS_64BIT_v5.34.4_05_07_2024.exe
Tecnomatix_17.0_KAWASAKI_AS_SUZUKI_64BIT_v1.3.4_05_07_2024.exe
Tecnomatix_17.0_NC_CODE_EMBRAER_64BIT_v1.17_05_07_2024.exe
Tecnomatix_17.0_NC_CODE_RIVETING_64BIT_v1.15_05_07_2024.exe
Tecnomatix_17.0_OLP_TOOL_64BIT_v16.4.3_05_07_2024.exe
Tecnomatix_17.0_YASKAWA_INFORM_64BIT_v6.57_05_07_2024.exe
Tecnomatix_2206_ABB_RAPID_64BIT_v5.28.2_05_07_2024.exe
Tecnomatix_2206_ABB_RAPID_VOLVO_64BIT_v5.18.2_05_07_2024.exe
Tecnomatix_2206_CLS_UPLOAD_64BIT_v1.15.5_05_07_2024.exe
Tecnomatix_2206_COMAU_PDL_64BIT_v5.7.1_05_07_2024.exe
Tecnomatix_2206_COMAU_PDL_VOLVO_64BIT_v2.16.1_05_07_2024.exe
Tecnomatix_2206_DEFAULT_64BIT_v2.140_05_07_2024.exe
Tecnomatix_2206_DUERR_ECOTALK_64BIT_v2.91_05_07_2024.exe
Tecnomatix_2206_FANUC_RJ_64BIT_v5.3.1_05_07_2024.exe
Tecnomatix_2206_FANUC_RJ_JAPAN_64BIT_v3.2.2_05_07_2024.exe
Tecnomatix_2206_FANUC_RJ_VW_64BIT_v4.0.1_05_07_2024.exe
Tecnomatix_2206_HHI_HRBASIC_64BIT_v2.1_05_07_2024.exe
Tecnomatix_2206_KAWASAKI_AS_64BIT_v5.34.4_05_07_2024.exe
Tecnomatix_2206_KAWASAKI_AS_SUZUKI_64BIT_v1.3.4_05_07_2024.exe
Tecnomatix_2206_NC_CODE_EMBRAER_64BIT_v1.17_05_07_2024.exe
Tecnomatix_2206_NC_CODE_RIVETING_64BIT_v1.15_05_07_2024.exe
Tecnomatix_2206_OLP_TOOL_64BIT_v16.4.3_05_07_2024.exe
Tecnomatix_2206_YASKAWA_INFORM_64BIT_v6.57_05_07_2024.exe
Tecnomatix_2402_ABB_RAPID_64BIT_v5.28.2_05_07_2024.exe
Tecnomatix_2402_ABB_RAPID_VOLVO_64BIT_v5.18.2_05_07_2024.exe
Tecnomatix_2402_CLS_UPLOAD_64BIT_v1.15.5_05_07_2024.exe
Tecnomatix_2402_COMAU_PDL_64BIT_v5.7.1_05_07_2024.exe
Tecnomatix_2402_COMAU_PDL_VOLVO_64BIT_v2.16.1_05_07_2024.exe
Tecnomatix_2402_DEFAULT_64BIT_v2.140_05_07_2024.exe
Tecnomatix_2402_DUERR_ECOTALK_64BIT_v2.91_05_07_2024.exe
Tecnomatix_2402_EFORT_XPL_64BIT_v1.13_05_07_2024.exe
Tecnomatix_2402_ESTUN_ERL_64BIT_v1.25_05_07_2024.exe
Tecnomatix_2402_FANUC_RJ_64BIT_v5.3.1_05_07_2024.exe
Tecnomatix_2402_FANUC_RJ_JAPAN_64BIT_v3.2.2_05_07_2024.exe
Tecnomatix_2402_FANUC_RJ_VW_64BIT_v4.0.1_05_07_2024.exe
Tecnomatix_2402_HHI_HRBASIC_64BIT_v2.1_05_07_2024.exe
Tecnomatix_2402_KAWASAKI_AS_64BIT_v5.34.4_05_07_2024.exe
Tecnomatix_2402_KAWASAKI_AS_SUZUKI_64BIT_v1.3.4_05_07_2024.exe
Tecnomatix_2402_NC_CODE_EMBRAER_64BIT_v1.17_05_07_2024.exe
Tecnomatix_2402_NC_CODE_RIVETING_64BIT_v1.15_05_07_2024.exe
Tecnomatix_2402_OLP_TOOL_64BIT_v16.4.3_05_07_2024.exe
Tecnomatix_2402_YASKAWA_INFORM_64BIT_v6.57_05_07_2024.exe
To Install:
Place Tecnomatix_<TecnomatixVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe into a folder ($Tecnomatix/downloads is suggested, where $Tecnomatix is the full path to the Tecnomatix installation).
Run Tecnomatix_<TecnomatixVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe.
The default installation point is C:\Program Files\Tecnomatix.
If you have any issues with the installation or support of these fixes,
please contact your local GTAC support group.
Sincerely,
Siemens Digital Industries Software