How to show/ add column for Hole Tolerances in Draft Hole table?

2024-09-13T03:38:02Z

Summary


Details

How to show/ add column for Hole Tolerances in Draft Hole table?

Solution

You can specify stack or limit tolerance to be added to the evaluated hole size or diameter in a hole table.

1. Click the Columns tab in the Hole Table Properties dialog box.

2. In the Columns list, click Size.

You also can click the Diameter/Thread column.

3. In the Property text box, click inside the underlined property text string that extracts hole size or hole diameter from the model.

Note: Underlined property text indicates a string whose value is eligible for formatting. Pink property text indicates a symbol code.

When the underlined property text string turns red, click the Format button.


In the Format Values dialog box:

a. Click Tolerance.

b. Select the tolerance type (Stack (/ST) or Limit (/LT).

c. In the Upper box, type the value for the upper stack tolerance or the upper limit value.

d. In the Lower box, type the value for the lower stack tolerance or the lower limit value.

e. Click OK.

The hole size property text string on the Columns tab is updated with the modifying property text code.


4. In the Hole Table Properties dialog box, click Apply to update the table.


Notes

11086245

KB Article ID# PL8798469

Contents

SummaryDetails

Associated Components