NX About the use of the Flat Pattern View option of PMI preferences.

2024-06-30T11:55:25Z
NX for Design

Summary


Details

The users cant understand the use case of the Flat Pattern View option of PMI preferences.

the users think the bend label set it as check ON but it is not displayed on the Flat Pattern View.


Solution

When you create a flat pattern, NX displays flat pattern information as PMI objects in the flat pattern view.

Using PMI preferences.

Sheet Metal>Flat Pattern>Flat Pattern View.

The Users can select flat pattern label settings from the Flat Pattern View of PMI preferences such as

[Bend Labels, Hole Details Labels, Joggle Labels, etc] those are wants to display as a PMI objects in the flat pattern view.

Users can configure the text that they want to display as  the PMI objects  from Flat Pattern View

Determine which information want to display in a flat pattern view.

Example:  as the information about Bend such as Bend Sequence ID, Bend Name, Bend Direction, and Bend Angle in the flat pattern view.

if Bend Direction : Check ON


In Flat pattern View dispalyed Bend Direction only.


KB Article ID# PL8798410

Contents

SummaryDetails

Associated Components

Drafting PMI Sheet Metal