Solid Edge 2024 Update 6 Announcement

2024-06-24T19:49:05Z

Summary


Details

June 24, 2024

Dear Solid Edge Customer:

Solid Edge 2024 Update 6 is now available for download.

We appreciate your continued business and participation in the software support process. Your feedback helps us improve Solid Edge and better serve your business needs.

Sincerely,

The Solid Edge Team

============

Release Notes:

============

Solid Edge 2024 Update 6

Version: 224.00.06.05

Download Solid Edge 2024 (2310) Updates

If clicking the direct download URL does not resolve in your browser, please go ahead, and navigate from the top-level Support Center.

===============

Email Notification:

===============

To receive direct email notifications for Solid Edge Updates, navigate to your Support Center Profile (https://account.sw.siemens.com/profile, scroll to Newsletter Subscriptions, and check the box for Software Field Bulletin

==========================================

This Solid Edge Update resolves the following PRs:

==========================================

===General===

PR 11078929: Installing 2024 Update 5 on the baseline release changes templates from ANSI to ISO.

===Assembly===

PR 10971651: Fastener system, Solid Edge crashes with customers custom.xml.

PR 10993942: Solid Edge crashed while replacing a part placed with the 'Match Coordinate Systems'.

PR 11055945: Solid Edge crashed when opening in simplify assembly mode and selecting Coordinate Dimension.

PR 10588544: Standard parts do not work with a Cloud-Enabled license.

PR 11063926: Solid Edge crashed when performing multiple Synchronous edits and returning to Ordered.

PR 11066716: After installing Update 5, the customer has various assembly files that will no longer open.

PR 11069487: In the customer's assembly, some part locations change when the Item number changes.

PR 11070154: Highlighted elements are deselected when switching Assembly Relationship Type.

PR 10994655: Different behavior depending on part or assembly when using the Create3D command.

PR 11057530: Solid Edge crashed when you Undo a 3D Curve command.

PR 11041106: Solid Edge crashed when pressing ESC to exit the 3D Curve command.

PR 11074968: Unable to use Find Components in Path Finder in a Floating Window

===Draft===

PR 11053096: The Esc key is not working in some cases.

===Part/Profile/Sheetmetal===

PR 11003046: A flattened blank from an imported step file shows the wrong dimensions.

PR 11066546: Updating a Drawing View associated with a Sheet Metal type document causes deletion.

PR 11069463: Crash while rotating a specific selection set in the Synchronous environment.

PR 11075258: Reproducible Solid Edge crash while saving legacy data.

===SEEC===

PR 11042312: Two datasets were created for the PDF.

PR 12022942: Sub-component changes are lost when checking out a read-only assembly.

PR 12018038: Reproducible crash when selecting a sub-assembly in Pathfinder.

PR 12023891: Model Views are not showing correctly in Teamcenter Viewer.

PR 10851847: Structure Editor terminating during "Save all as..." of a large assembly.

PR 12024727: SEEC does not support Multiple revisions within hidden & unexpanded structures.

===Solid Edge Data Management===

PR 10813729: Releasing a file in the release library path moves it to the root folder.

===TechPub===

PR 10839139: The selected line style was not exported to vector files correctly.

PR 11055308: Weldment selection does not transfer to html output..

PR 11075354: The model is displayed in HTML with a distance in an additional 3D window.

PR 11075484: Illustration part list, fill functions apply a color to the background and to the text.

PR 11075557: Scaling of the model in a 3D publishing/HTML file causes it to become not visible.

===Translators===

PR 11003098: When saving a large assembly as JT fails.

PR 11044508: The scale of the model when converting to STL is incorrect using the millimeter import option.

PR 11057976: Save Copy as XML is not creating an XML file.

PR 11054703: SolidWorks Data Migration hanging/not completing for SLDDRW files.

PR 11069256: Inventor migration is failing.

KB Article ID# PL8797448

Contents

SummaryDetails

Associated Components