About "Redefine Constraints" dialog of PTS

2024-06-30T12:30:48Z

Summary


Details

How to launch the "Redefine Constraints" dialog of PTS

Solution

To launch the "Redefine Constraints" dialog of PTS use the typical procedure as below:

1. Create a sample assembly file.

2. Create few Assembly Constraints.

3. Remember the Assembly Constraints if they are not already.

4. Make assembly component as displayed part > Switch to "Product Template Author" application

5. Configure User Interface > in Properties set as below.

Launch redefine constraints : True

Allow quick access to the template : No Quick Access

6. Switch to Modeling application

7. Add the component to the assembly.

The "Redefine Constraints" dialog will be launched.

KB Article ID# PL8797299

Contents

SummaryDetails

Associated Components