About Examine Geometry Check Mate test tolerances

2024-06-30T12:13:27Z

Summary


Details

Perform an Examine Geometry Check Mate test as below.

Menu > Analysis > Check-Mate > Set Up Tests.

Tests (tab) > Modeling > Examine Geometry > Select any test from the available tests for e.g. "Bodies - Face-Face Intersections"

Select the test "Bodies - Face-Face Intersections" from the Chosen Tests > Customize.

Note that in the Customization dialog, there is no option to set the tolerances for the tests.

From where does the Examine Geometry Check Mate test refer to the tolerances?

Solution

Each Check-Mate test under the Examine Geometry Category refers to the tolerances as set in the Examine Geometry UI dialog.

KB Article ID# PL8797285

Contents

SummaryDetails

Associated Components