Solid Edge Unable to Create Physical Pipe Threads in Solid Edge

2024-06-12T09:03:47Z
PART/SHEETMETAL

Summary


Details

Users are unable to create physical pipe threads in Solid Edge. When attempting to do so, the command for creating physical threads is greyed out and unavailable.

Steps to Reproduce:

1. Create a threaded hole in Solid Edge.

2. Select a pipe thread for the hole.

3. Attempt to create a physical thread from the pipe thread.

4. Observe that the physical thread command is greyed out.

Solution

This behavior is by design. Solid Edge does not currently support the creation of physical pipe threads. There is an existing Enhancement Request (ER) for this functionality. Please submit a new Support Case to be attached to the master ER for tracking and consideration in future updates.

KB Article ID# PL8795754

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES