Sample Mill Turn Simulation kit Showing a Part Pull Out

2024-08-09T17:59:43Z

Summary


Details

Are there any sample simulation kits along with a sample part showing how to do a part pull-out on a two spindle turning machine?

Platforms
  • Windows x64 11
Release Versions
  • NX V2406
Solution

1. Open ...\nx2406\MACH\resource\library\machine\installed_machines\sim15_millturn_9ax\cam_setup\smpl_sim15_2ch-mlltrn_sinumerik_mm.prt

2. Select the SYNCH-GROUP Program Group.


3. Press Simulate Machine


4. Set Machine Code Based Simulation.


5. Turn 0n Material Removal and Play.

6. When the PART-PULL-OUT operation is simulated part pullout is done. This Generic motion operation contains the Sub-Operations that adds this motion.


Notes

KB Article ID# PL8795641

Contents

SummaryDetails

Associated Components