Solid Edge No Limit on License Borrowing Frequency

2024-06-10T19:19:21Z
SETUP

Summary


Details

A customer asked about the maximum number of times a license can be borrowed in a year. The customer has multiple delegations to various client sites and requires the ability to borrow a license for 1-2 weeks each month while working offsite. They need to ensure there are no restrictions on the frequency of license borrowing from their server.

Solution

There is no limit to the number of times a floating license can be borrowed in a year. License borrowing subtracts a license from the pool of available floating licenses until the borrowed license is returned. This means users can borrow licenses as many times as needed without any restrictions.

KB Article ID# PL8795200

Contents

SummaryDetails

Associated Components

SETUP: LICENSING