Crosshatch not created in PMI section view

2024-06-10T23:35:32Z

Summary


Details

It is not created in Section view even though "Display Crosshatch" is specified.

Reproduced Steps:

1. Create a box solid ( with X=20, Y=10 and Z=0.2)


2. File > PMI > PMI Section View > Section View > Crosshatch > Display Crosshatch =ON


3. Menu > PMI > PMI Section View (One Plane, Section Plane/Plane = Y)



Solution

This behavior is working as designed.

In PMI Section View, there is a tolerance setting used for Crosshatch creation. If it has a thickness less than the specified value, the crosshatch will not be created.

The Tolerance setting:

File > Preferences > PMI > Annotation > Crosshatch/Area Fill > Boundary Curve > Tolerance


Current Tolerance Value = 0.25

Thickness of solid in Z direction = 0.2

In this case, setting a tolerance value less than 0.2 will create a crosshatch.


Notes

**Please refer to PL8795041 for Japanese article.

Release Versions
  • NX V2312
  • NX - PMI V2312
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8795043

Contents

SummaryDetails

Associated Components