PCB Exchange fails to make incremental changes

2024-06-21T20:47:16Z

Summary


Details

Starting a PCB Design from NX in managed MFK environment, the User is able to create a board assembly and create a baseline IDX file for expedition consumption. However, when they import the incremental change "*.idx" from expedition back into NX, it fails to bring in any components or make any changes.

Solution

The following settings are required in the pcbx_ug_model.ini file;

o NxWriteTcPartAutoGenerateItemID = Yes

o NxWriteTcAssemblyAutoGenerateItemID = Yes

Notes

Ref: PR 10535123

KB Article ID# PL8794660

Contents

SummaryDetails

Associated Components