Adjusting Decimal Precision in Solid Edge Modeling Environment

2024-06-05T19:57:49Z

Summary


Details

Users in the Solid Edge modeling  environment can see up to 7 digits after the decimal separator, but can only change up to 4 digits. The user asked about the default modeling tolerance in Solid Edge and if it can be changed.

Solution

1. Check and Adjust Precision Settings:

  • Navigate to Solid Edge Settings.
    • Go to Options -> Units.
      • Under Base Units, set the Precision to 7 decimal places. This setting allows users to view more precise dimension values in the dialogs.

        2. Verifying Changes:

        • After adjusting the precision setting, verify that the increased precision is reflected in the user interface dialogs.

          These steps allow users to view and utilize more precise dimensions in their Solid Edge models. 

          KB Article ID# PL8794656

          Contents

          SummaryDetails

          Associated Components