Solid Edge MBD Installation and Licensing

2024-06-05T19:38:07Z

Summary


Details

A user inquired whether Solid Edge Model-Based Definition (MBD) requires a separate installation or if it is included in the Solid Edge installation package.

Solution

Solid Edge MBD is included as part of the core Solid Edge installation. There is no need for an additional software installation to use MBD. However, a valid license for MBD is required to activate and use this feature.

KB Article ID# PL8794652

Contents

SummaryDetails

Associated Components