Export Options in 3D Print Tab

2024-06-05T07:11:59Z

Summary


Details

Users reported that the Options button is missing from the Export command window in the 3D Print tab. This prevents users from setting the mesh quality for their export. However, the Options button appears as expected when using the Save As -> STL or 3MF command.

Solution

The absence of the Options button in the Export command window within the 3D Print tab is by design. The export options for STL or 3MF files are configured through the main application settings. To access these settings, follow these steps:

  1. Go to the main application page.
    1. Navigate to Settings.
      1. Select the Options button.

        By adjusting the settings here, you can set the desired mesh quality for your exports. These settings will apply to all export operations, including those initiated from the 3D Print tab.

        KB Article ID# PL8794502

        Contents

        SummaryDetails

        Associated Components